AXIS#.PL.FBSOURCE
Description
This parameter determines the feedback source that the position loop uses.
Value | Description |
---|---|
0 | Defers selection to AXIS#.IL.FBSOURCE - this is the default, and uses the value which is being used for commutation |
1 | Selects FB1 (connector X1) |
2 | Selects FB2 (connector X2) |
3 | Selects FB3 (connector X23) |
4 | Selects FB4 (connector X21) |
5 | Selects FB5 (connector X22) |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 5 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.PL.FBSOURCE | 0x500C | 0x8 | USINT | - | - | RW | False |
AXIS2.PL.FBSOURCE | 0x510C | 0x8 | USINT | - | - | RW | False |